Industry Online Support
Technical Forum
6/24/2014 2:52 PM | |
Posts: 6 Rating:
|
I am trying to make a prototype for a new software approach, and currently I'm working on the alarm. I would like to use the ALARM_DQ blocks in a 317 CPU (any) in combination with a couple of panels (377, TP1200, etc). I build myself a TIA v12 upd 5 project with the hardware described. I used the following sources: - https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=62121503&caller=view - https://support.automation.siemens.com/WW/llisapi.dll?func=ll&objid=36050550&nodeid0=11599011&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW The last one is a Simatic Manager solution, I downloaded the example projects which worked. I reproduced the solutions, and these worked as well. Currently I have 1 FB with 2 ALARM_DQ blocks. The alarms message show under PLC Alarms. I added the HMI's and added an alarm view on both. The connections are configured (ethernet, mpi) but to my suprise there is no setting for enabling the ALARM_S option (which SM5.5 has). When I run both the PLC and TP in simulation, I dont get any alarms displayed on the TP. Can anyone give me a lead what to look for, as the documentation doesnt help me anymore. Or better yet, maybe an example project! TNX! |
6/25/2014 10:57 AM | |
Posts: 6 Rating:
|
Hi Cicero! You mean the settings on the DB parameters? See attachment regards, Ron |
Last edited by: ronski at: 6/25/2014 11:02 AMedit |
|
Follow us on