8/3/2017 9:19 AM | |
Joined: 8/3/2009 Last visit: 2/14/2025 Posts: 14758 Rating:
|
Hello TomazCKP -> First of all you cannot pull out the USB Stick or SD Card while the Panel uses the Files on it!!!! -> You have to use the Systemfunktions: StopLogging (for every Log) -> CloseAllLogs Then you can use the Logfiles or pull out the USB Stick. If you plugin the USB Stick again the best would be to restart the Panel because the Panel has no 100% Plug and Play functionality like a normal windows System. But in every case you have to OpenallLogs and then StartLogging to sour log again. (Or you stop runtime and if the USB STick is present again you can start Runtime again.) Here you can find a good solution: https://support.industry.siemens.com/cs/ww/en/view/63042926 the Very Best would be to use the SD Card for Logging (and do not pull out) and use the FAQ to create an Export File to the USB Stick. Then the USB Stick has no influence on the Runtime. Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/3/2017 3:34 PM | |
Posts: 20 Rating:
|
Hi Murof, thanks for the reply. I will use SD card for alarm loging like you suggest. And try to make a function to transfere alarm log to USB key. Thanks BR |
Follow us on