8/22/2017 6:15 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 112 Rating:
|
Dear All, I am trying to perform a simple test on ALARM_S, based on a manual " Configuration of Messages and Alarms in WinCC (TIA Portal)". But the problem now is that the Alarm_s block has a Return Value of 8084 "8084 With the current and the previous "ALARM_S", the alarm-triggering signal SIG has the same value." - this is the Return value description in the pdf. And I cant understand this sentence from help " You must make sure that you call the instruction only when the value of the alarm-triggering signal SIG is inverted compared to the last call. If this is not the case, then this situation will be indicated in RET_VAL and no alarm will be sent. With the very first call of the instruction you must ensure that the value "1" is applied at the SIG input"
I have attached screen shots of this issue. Thanks AttachmentDesktop.zip (49 Downloads) |
Last edited by: Satheesh290692 at: 8/22/2017 7:36:09 AMLast edited by: Satheesh290692 at: 8/22/2017 7:36:53 AMThanks |
|
8/22/2017 9:04 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 112 Rating:
|
Or If there is any simple test program please share! |
Thanks |
|
9/1/2017 9:26 AM | |
Joined: 9/1/2005 Last visit: 4/10/2025 Posts: 4113 Rating:
|
closed cause question posted twice. The second thread with the subject The Alarm_s block has a Return Value of 8084 is published within the conference STEP 7 (TIA Portal) Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on