Industry Online Support
Technical Forum
10/29/2013 1:52 PM | |
Joined: 10/8/2008 Last visit: 9/20/2024 Posts: 43 Rating: (0) |
Hi all, I use a s7-1500 PLC and a TP700 configuring the alarm in the PLC i use the Program_alarm an the Get AlarmState. when the alarm is active i can see it in the alarm window on the TP700 I used the standart setup for the TP700. What not seems to work is flashing of the second grafic on the left side (alarm active, or new alarm) in some other post someone is refering that the ! should flash. Has somebody experiance with this. Thanks Jan AttachmentScreen.zip (238 Downloads) |
10/31/2013 8:38 AM | |
Joined: 10/8/2008 Last visit: 9/20/2024 Posts: 43 Rating: (0) |
Hi Nelliyan, thanks for the reply. Wesolft the problem. because we are not using the errors (alarm class), but instead the acknowledge the corresponding grafic doesn't pop up You have to v the intems, see download. Thanks,,Jan AttachmentGlobalscreen.zip (261 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on