6/30/2015 2:49 PM | |
Joined: 11/19/2013 Last visit: 3/6/2025 Posts: 3 Rating:
|
Hi i'm using TIA V13 SP1. HMI comfort 700 How can i activate a pop-up with an alarm? if alarm is set, the pop-up should appear and the alarm should be confirmed if you push a button in the pop-up. In my HMI alarms > dicrete alarms > properties of specific alarm > events, i can't find the function "ShowPopUpScreen" Is it not available or am i doing something wrong? Thx |
6/30/2015 5:23 PM | |
Joined: 10/21/2013 Last visit: 3/8/2025 Posts: 421 Rating:
|
Hi merco, By default the alarm view ll be configured in global screen which appears when alarm occurs It is closable and has acknowledge button too.... It cannot be configured as pop up |
7/1/2015 7:31 AM | |
Posts: 1299 Rating:
|
Hello, I think it's not available. But you can write a little vbscript with the function "ShowPopupScreen" and call this script on the event of the alarm. K!ke |
7/1/2015 10:07 AM | |
Joined: 11/19/2013 Last visit: 3/6/2025 Posts: 3 Rating:
|
Ok i'll try the alternative then. Thx fot the feedback |
Follow us on