10/29/2014 6:54 PM | |
Posts: 24 Rating:
|
Hello! I use SIMATIC S7-1214C PLC. I am controlling with it a farm (lights and food lines). I bought already a GPRS modul CP1242-7. I want the PLC to send me a SMS when something is wrong. For example if the Input I0.3 is TRUE then it should send me a SMS with text "Alarm1". I´m not an expert, therefore I would need help. I programmed it already as the guys from Siemens said, but it still doesn’t work. ( https://www.youtube.com/watch?v=56xN8d7TmVc ) The configurations are most probably ok, becasuse if I send "CPDIAG" to GPRS modul I receive a sms with information about the controller status... I did exactly the same as the Siemens person said. But it doesn’t work. I know what I should do, but for me it´s not clear what I should but into “data” (TC_SEND)(Image1). When I put the input REQ (TC_CON)(Image2) on TRUE then nothing happens (all outputs are FALSE). I dont know if the Datablock for TC_CON is ok(Image3). Can anybody help me?? Please! Thank you very much! Attachmentpictures.zip (48 Downloads) |
Last edited by: Min_Moderator at: 10/30/2014 11:48 AMLast edited by: Min_Moderator at: 10/30/2014 11:47 AMMove pictures in attachment |
|
Follow us on