5/27/2021 8:38 AM | |
Joined: 12/18/2014 Last visit: 12/22/2024 Posts: 34442 Rating: (4294)
|
Lit the RUN/STOP LED with a other color (red, orange, yellow)? |
5/27/2021 8:41 AM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating: (0) |
No, it doenst give any light. |
5/27/2021 8:48 AM | |
Joined: 4/28/2021 Last visit: 6/27/2022 Posts: 32 Rating: (0) |
Already tried that, i measured 24V on L+ and M. |
5/27/2021 9:04 AM | |
Joined: 6/19/2019 Last visit: 12/17/2024 Posts: 706 Rating: (77) |
Yes it can be. See also in PDF or you connected earth and cable shielding? If your slider was also in so you will also must burn and LOGO also? I think if from one power supply you give + and M to your LOGO and extansion modules then you must burn all system which is 24VDC AttachmentSIMATIC LOGO! Manual - Logo_e.pdf (407 Downloads) |
Last edited by: Mr.V at: 05/27/2021 09:09:29 |
|
This contribution was helpful to1 thankful Users |
Follow us on