6/2/2013 11:21 AM | |
Posts: 8946 Rating: (999) |
Hi volks, please have a look at http://en.directupload.net/ It provides a fast, free-of-charge upload of pictures and pdf-files. That makes it easy to get a picture or a manual also if you are not logged in to the forum. |
This contribution was helpful to1 thankful Users |
6/2/2013 9:09 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Hello Jürgen, I just tried that once to have a picture in body of message in the post.I did not provide back up of that picture as an attachment in the forum and space provider deleted the file.This was sad and I simply delete the whole thread because it was meaningless without that. We can provide both i.e back up in the forum or some in other space providers but files in the second option may not last forever. We may ask moderators to make downloading possible without being "logged in" but I am sure they are against this because they may loose this dramatically increasing rate of registered members. Best regards Hamid Hosseini |
This contribution was helpful to1 thankful Users |
6/14/2013 1:18 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
Hello, and thank you for your ideas. We moderators think that it is still better to upload your files directly in forum. Being registered on other sites may be a possible solution to have the files staying for a long time, but it is never sure how long this will be. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
7/5/2013 8:39 AM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
That's indeed a very understandable reason but in rare cases that you want to share something bigger, IBN's way is a good alternative. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
7/5/2013 11:09 AM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
That's very true. On the other hand, I've seen a few times before that an unavailable file was re-uploaded by request by other members. I keep most interesting downloads from this forum saved on a stick and would be happy to reupload some if I notice someone requesting one of these... but as said before, it's best to keep it all on the forum, if possible. |
B r g d s , |
|
7/6/2013 2:30 PM | |
Posts: 621 Rating: (10) |
that website is not opning in my internet login i will check it next week... |