7/18/2018 8:30 AM | |
Posts: 9 Rating:
|
Hi i have connected a flowrate sensor which runs on 5V to my LOGO!8 and i realise my LOGO!8 could not pick up the signal as my current of the sensor is too low. For some reason, the current i picked up using a multimeter is only 0.03mA. What should i do for my LOGO!8 to be able to read the sensor and display on my LOGO!* screen. Attached is the program which is running on my LOGO!8. Is there also a way to improve my program to read the flow rate from a normal water tap accurately? |
7/18/2018 9:07 AM | |
Posts: 9 Rating:
|
The Siemens order number is 6ED1 052-1FB00-0BA8 |
Follow us on