1/3/2008 10:22 PM | |
Joined: 1/7/2006 Last visit: 11/21/2020 Posts: 2705 Rating:
|
Hi Donflore, On your question is the following data there, how do you connect a potentiometer to the analog module 6ES7 331-1KF0.-0AB0?
More information is available in the manual "SIMATIC S7-300 Programmable Controller Module Specifications " in Entry ID 8859629. |
Last edited by: Late at: 03.01.2008 22:24I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/4/2008 3:55 PM | |
Posts: 21 Rating:
|
Hi Late, Thanks for the answer to my question, it will really help me ... Bye |
1/6/2008 10:07 PM | |
Joined: 1/7/2006 Last visit: 11/21/2020 Posts: 2705 Rating:
|
Hi Donflore, As far I could see the connections are ok. The power is coming from the 5V of the backplain. Yes, AI and AO are a little bit difficult, but when you are reading the handbooks then you might learn a lot of analog values, it is not difficult. Please look to the getting started of the analog cards to make the right decision.... SM331; AI 8x12 Bit Getting Started part 1: 4 -20mA SM331;AI 8x12 Bit Getting Started Part 2: Voltage and PT100 SM331; AI 8 x 12 Bit Getting Started part 3: Thermocouples |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/7/2008 6:43 PM | |
Posts: 21 Rating:
|
Hi Late... Thanks again for the answer ... Yes ... i'll spend more time reading the handbooks ... Bye, bye |
Follow us on