8/16/2018 8:49 AM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31546 Rating:
|
I have created the program times according to your specifications. Start the simulation and let the actual value increase. Output Q1 is permanently on, since it is below 90. If the transition from 89 to 90 now occurs, it came a pulse for output Q1. However, it can not be recognized as an independent pulse since it only acts as an extension of the on-time of Q1. AttachmentKarthikk.zip (128 Downloads) |
This contribution was helpful to
1 thankful Users |
8/17/2018 6:25 AM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31546 Rating:
|
The new Version.
AttachmentKarthikk_V2.zip (112 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on