6/14/2014 10:13 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello, in capture 3.8 you will fine a limiter. Depend on the limit, you can set a output. Zako AttachmentFH2_0111_eng.pdf (59 Downloads) |
6/15/2014 3:49 AM | |
Joined: 3/15/2011 Last visit: 3/20/2024 Posts: 134 Rating: (9) |
Hello everybody, In SINAMICS S120 or other series can we do a numerical or logical operations on analog inputs ? For example: We have an analog input 4-20 mA (using TM31 or other modules) and we want to trigger a digital output or anything else when the value of the analog input reaches 10 mA then trigger other thing we it reaches 15 mA. Best regards Ali ALKARN
Hi, you can use NSW and limiter(free function block) to accomplish your task.i did this few years back.Hava a look in attachment. Regards Ashutosh Attachmentscan0031.pdf (64 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on