1/19/2016 2:27 PM | |
Posts: 163 Rating: (2) |
And what is meant by config A and B? |
1/20/2016 7:43 AM | |
Posts: 163 Rating: (2) |
Thanks... Do you mean that I should give it only +-10v dc? I am tapping power from my 24v dc. should I use voltage regulator?
Thanks |
1/20/2016 8:22 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
Hi idir, the 7KB02 does not only support a measurement of +/-10V. You can use resistance measurement. The resistance input ranges are 150/300/600 Ohm. It is not recommended to use 24V on voltage input. The destruction limit is: max. 20 V continuous; 75 V for the duration of max. 1 s (duty factor 1:20). See the technical data in the manual you already have, page 392 and further. hope this helps, regards, |
FCK WAR! |
|
Follow us on