10/20/2015 5:54 PM | |
Posts: 8946 Rating: (999) |
No. Analog voltage Output supports only a larger minimum resistor. Depending form specifications, the Minimum is mostly approx. 1000 - 10000 Ohm. |
10/20/2015 6:11 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33423 Rating: (4148) |
For Logo ÁM2 AQ look at attachment.
AttachmentLOGO! 8 Soft manual 0BA8 06_2014_side_311.pdf (171 Downloads) |
10/20/2015 6:56 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33423 Rating: (4148) |
In attachment there is a possible actuator from Belimo.
AttachmentSM24-SRS.pdf (168 Downloads) |
10/20/2015 8:43 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33423 Rating: (4148) |
Here is a simple program with the minimum requirements. The setpoint can be changed directly from the display.
AttachmentCircuit Diagram1.zip (211 Downloads) |
Follow us on