12/27/2018 9:41 PM | |
Posts: 121 Rating:
|
This produced the exact same result Thanks for trying |
12/27/2018 9:44 PM | |
Joined: 12/18/2014 Last visit: 3/26/2023 Posts: 29498 Rating:
|
No. Then make you not the same as I. |
This contribution was helpful to
1 thankful Users |
12/28/2018 7:07 AM | |
Joined: 12/18/2014 Last visit: 3/26/2023 Posts: 29498 Rating:
|
I can not understand your devotion, something is different with you. I have set the voltage at the analog input so that the analog input after the conversion shows exactly 3222 units. The measured voltage at the analog input is 1.171 VDC (with a set measuring range of 2 VDC). Attached is an online screenshot with the values and the complete calculation. AttachmentPressure.pdf (66 Downloads) |
12/28/2018 7:55 PM | |
Joined: 12/18/2014 Last visit: 3/26/2023 Posts: 29498 Rating:
|
If yo mean... |
Follow us on