7/9/2021 8:19 AM | |
Joined: 12/13/2019 Last visit: 8/16/2022 Posts: 21 Rating:
|
Hello, Anyone knows why analog treshold trigger is not able to react to the set value ( -120) ? I have attached the diagram. In simulation mode- If I slide the analog input through the entire range, the trigger is not able to change to ''positive'' , even if the set threshold value has been exceeded. It only change to positive if I change value by clicking through the Input range manually by mouse, passing point -120. This way it works. I am trying to built a FBD which monitors 0-4V output from frequency drive, and when a certain voltage is exceeded the latching relay will stay on until RESET. Thanks, George AttachmentCurrent treshold exceeded (forum).zip (154 Downloads) |
7/9/2021 2:28 PM | |
Joined: 12/13/2019 Last visit: 8/16/2022 Posts: 21 Rating:
|
OK, that explain then. Thanks. |
Follow us on