11/12/2006 4:27 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, When you look at Connecting a potentiometer on the pages by Siemens then you have a idea to connect a potentiometer. Also in the handbook SIMATIC S7-300 Programmable Controller Module Specifications you may find how to measure a potentiometer. If there is something wrong with the signal, for example a to low or high resistor then you may get difficulties with the measurement and a overflow or underflow may come. It is also very important to have the M and the Earth very good for the analog signals. |
Last edited by: Late at: 11/12/2006 4:31 PMHandbook link was not right... I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|