3/28/2019 6:02 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi OMKRIS2017, 1. U will need to use dedicated CP for point to point interface e.g. CP440. MPI port can't be used for this purpose. 2. The pin out diagram is provided in the respective manual. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to
1 thankful Users |
4/2/2019 9:13 AM | |
Posts: 3093 Rating:
|
Hello, Regards, |
6/17/2019 4:05 PM | |
Joined: 1/1/2017 Last visit: 3/27/2025 Posts: 339 Rating:
|
Hello, Cameback after a long time. Now I've used Anybus Profinet to RS-485 converter for communication between the S7 412-2 PN PLC & ANDON Display. The Anybus device I've successfully installed the GSD & configured it in the TIA V1 SP1 software in which I'm doing the logic. Now one strange problem I'm facing. The issue is that whenever I'm assigning Input/Output address length like 8bytes or 32 bytes or 27 bytes the Anybus device is showing fault, it's 02 no LED get's continuously blinking RED. But whenever I'm deleting the address range then the deice LED is glowing GREEN. I'm confused that why such peculiar thing is happening. I'm attaching the Anybus device data specs for reference, it's very simple but can't understand that why in TIA such issue is happening. Waiting for response. Is there any other method of configuring the Anybus card or some other reasons are there for this issue. Also I forgot to mention that no data is getting exchanged in the address I've assigned in the Anybus IO's. Regards OmKris Attachmenthms-sp0843.pdf (63 Downloads) |
6/28/2019 11:23 AM | |
Joined: 1/1/2017 Last visit: 3/27/2025 Posts: 339 Rating:
|
Dear Team, Thanks for your support! The problem has been resolved! Regards OmKris |
Follow us on