12/1/2010 7:10 AM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
Hello Ganes10
hopefully in development, but I'm afraid to say that there are NO DPV1 capable S7 300 CP's available at this moment in time.
I wishI could tell you that you are wrong, but youare (unfortunately) correct.
- Use the S7 300's CPU onboardDP port - Consider using a 319 CPU which offerstwo onboard DPV1 capable ports - Use a 400 (its Profibus CP's support DPV1) - Use only DPV0 functionality of theconnected DPV1 capable DP Slave Some additionalinfo is available at the links below: Which SIMATIC S7 masters support the PROFIBUS DPV1 additional functions? How can you tell whether your S7-300/400 master supports DPV1 functions? What should you watch out for when configuring a CP342-5 as DP master? |
Cheers |
|
Follow us on