8/17/2015 2:40 PM | |
Posts: 116 Rating: (2) |
what do you mean with " can it be that there was alway a IP was set? " |
8/17/2015 4:32 PM | |
Posts: 116 Rating: (2) |
Hi Christoph, Here is a result. 1_xx : they connect laptop to Siemens switch (one port connect to Siemens HMI, one port to X120 of D435) 2_xx: they connect directly to X120 of D435 Nothing reply at all? AttachmentProneta.zip (196 Downloads) |
Last edited by: Tikki at: 8/17/2015 4:34:08 PM |
|
8/17/2015 4:55 PM | |
Posts: 116 Rating: (2) |
I believe they did connect to Simotion controller. But I doubt with result. do I need to consider cross cable with direct connect to D435? |
8/17/2015 5:43 PM | |
Posts: 116 Rating: (2) |
Christoph, We got 8 !!! at 7-segment display |
8/17/2015 6:11 PM | |
Posts: 116 Rating: (2) |
So, 8 and 8. (8 dot) without middle segment flicker is same then ? How to fixed it? |
8/17/2015 6:13 PM | |
Posts: 116 Rating: (2) |
shall I try this ? from your previous answer What's happen if you put the PLC switch to stop and powerON? |