9/17/2013 6:56 AM | |
Posts: 11 Rating:
|
Dear All. There is a 400H Configuration where there are 8 remote ET 200M Redundant stations and two Y-Links . The input and outputdata is within 244 bytes and distance between nodes is less than 20 meteres There are 2 Y-Links:1. In Y-Link 1: there are 14 Siemens drives working fine, but introduction of one more drive/Anybus device gives bus fault.2. In Y-Link 2: there are 13 drives and 1 Anybus device are working fine. Please let me know if with the present configuration, we can connect the 1 Anybus device on Y-Link 1 and what needs to be done to connect the same. AttachmentY-Link.zip (65 Downloads) |
Follow us on