3/1/2016 4:41 AM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (347)
|
Hi, Picture : @PG_OpDi01_STANDARD.pdl_Triggers Function : Function csoQCInterlock_Index_Trigger(ByVal Item) Line : 14 Error : Variable is undefined: 'APL_GetIndexForIntlkQualityCode' This means that in the picture @PG_OpDi01_STANDARD.pdl, there is a trigger function in the object "csoQCInterlock" name of the functions is "Index_Trigger". inside this function at line 14 there is a call to 'APL_GetIndexForIntlkQualityCode' which is not present in your project. you must add this global function in your project. This function is defined in APL_VBScripts.bmo file. you need to add this file in your project. save it. you may need to deactivate your runtime and active again. please see attachment. AttachmentAdd_APL_script.zip (56 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
This contribution was helpful to1 thankful Users |
3/2/2016 1:36 AM | |
Joined: 12/24/2007 Last visit: 5/15/2024 Posts: 26 Rating: (0) |
Thank you, I checked the global script and the file seems to be there. AttachmentAPL.zip (51 Downloads) |