Industry Online Support
Technical Forum
3/4/2013 10:46 AM | |
Posts: 19 Rating: (0) |
Hi everyone, I would like to know if it possible to use the arabic language in a WinCC Advanced V11. I saw a thread (the end of the thread) for WinCC Flexible : Here I can't see the arabic language in the language list with a comfort panel (like TP900) project or a PC-RT project. So how to do this? Remark: the arabic language is installed on my PC (Windows 7 64 bits) |
Last edited by: MAIDEL at: 3/4/2013 10:51 AMLast edited by: MAIDEL at: 3/4/2013 10:50 AMLast edited by: MAIDEL at: 3/4/2013 10:48 AM |
|
3/4/2013 11:49 AM | |
Posts: 3037 Rating: (192)
|
Hello, Panels with Windows CE as operating system do not support fonts written from right to left. Which languages are available in WinCC flexible? A Comfort Panel uses Windows CE as operating system. Tweety I check the catalog ST80 for project languages of Comfort Panels. Arabic language is not possible with Comfort Panels. |
Last edited by: Tweety at: 3/4/2013 12:03 PM |
|
3/4/2013 3:37 PM | |
Posts: 19 Rating: (0) |
ok thank you Ayman, I'll check this |
This contribution was helpful to1 thankful Users |
Follow us on