3/5/2020 11:33 AM | |
Joined: 7/9/2015 Last visit: 2/3/2023 Posts: 3289 Rating:
|
Hi, I don´t know this Arduino PLC but you can use Analog Input 0-10V of S7-1200 modul. But so you have only a small measurement area of 0 to 1328 inc for 0-5V. Perhaps you can connect over TCP? Please check this entry: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?Regards, Towome |
If my post was useful, please rate me - thank you! |
|
3/5/2020 11:49 AM | |
Posts: 5 Rating:
|
Thank you! So we can use that 5V, no need to amplify but being penalty from 27648 to 0-1328? Just any way to communicate Arduino with S71200? Not about Profines or Profibus, sir! Just about an idie of my project. Sorry about my English!
|
Follow us on