7/13/2022 6:12 PM | |
Joined: 6/12/2017 Last visit: 9/12/2022 Posts: 2 Rating:
|
Are we able to import the MPC / APC library into an S7-1500, and if not - what level of controller is required to support these add on instructions. Working with an S7-1500 + WinCC deployment, but not necessarily a PCS7 installation - but I was hoping to utilize the MPC library for some of their loops. If one were to upgrade the necessary controller to an MPC compatible version (ie: S7-300/400) (assuming it's compatible with the remainder of the infrastructure) - will the MPC library be usable without a specific PCS license or something ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 07/14/2022 09:58:29New subject after splitting |
|
Follow us on