3/2/2017 2:54 PM | |
Posts: 10 Rating:
|
Hi all, i'm having troubles with area pointers. I have only a s7 1200 and a ktp900. I'm using recipes and i need to configure these pointers because recipe viewer go to "empty recipe" randomly. Im trying to view some data exchange betwen plc and hmi but i only have good results with "Coordination" point who has length = 1 and i can use a word of the global db . With the anothers pointer i need to use an array but i cant see communication and the recipes go to blank every random time. I have seen a lot of threads here, following all the leads but i cant get the correct answer. Im going to attach some print screen, thanks in advance. PD: I have try it with global addressing and absolute, changing the configuration of the db but no results. Also try Word data type and UINT on DB. PD2: The File is a .RAR renamed to .ZIP. AttachmentCOMM ISSUES.ZIP (135 Downloads) |
3/2/2017 2:56 PM | |
Posts: 10 Rating:
|
All another aspects of communications are working perfectly. |
Follow us on