3/26/2013 4:23 PM | |
Posts: 3037 Rating:
|
Hello, Where do you change this array? in your PLC project? Can you explain more about your problem? Tweety |
3/27/2013 1:29 PM | |
Posts: 3037 Rating:
|
Hello, Do you use WinCC V11 SP2 Update 5? Which runtime do you use? Professional or Advanced? Updates for STEP 7 V11 SP2 and WinCC V11 SP2 Service Pack 2 for WinCC V11 How do you migrate tags from STEP 7 V11 to WinCC V11? Tweety |
3/27/2013 3:08 PM | |
Posts: 3037 Rating:
|
Hello, You think it is a bug, you should install Update 5 for WinCC V11 SP2. Updates for STEP 7 V11 SP2 and WinCC V11 SP2 Tweety Do you use a HMI connection between your plc and runtime? |
Last edited by: Tweety at: 3/27/2013 3:10 PM |
|
3/27/2013 3:52 PM | |
Posts: 6 Rating:
|
I have just installed the update 5 last week. I use the TCP/IP connection between PLC and Pc with runtime. |
3/28/2013 11:09 AM | |
Posts: 3037 Rating:
|
Hello, You can see more about HMI connection in the manual chapter 8.1.3.2. WinCC WinCC Comfort/Advanced V11.0 SP2 Tweety |
4/2/2013 1:39 PM | |
Posts: 3037 Rating:
|
Hello, You do not have an S7 1200. I test an array of S7 300 with WinCC Runtime. It works well. You can start a Support request. Tweety |
Follow us on