5/1/2009 5:52 PM | |
Posts: 26 Rating: (0) |
Is the master call or the slave response structured differently when communicating to an AS-i safe slave than it is to a standard slave? |
5/4/2009 8:38 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, The safety-related design of AS-Interface was standardized for all manufacturers in the "Safety at Work" consortium (sub-group of the AS-i International Association) (see AS-i-Spec. 3.0). It is marketed by Siemens under the copyrighted name "ASIsafe". The concept allows both standard and safe data to be used in one single bus system. In this manual, in chapter 9, the basics of Asisafe are explained http://support.automation.siemens.com/WW/view/en/26250840 |
Best regards |
|
Follow us on