3/14/2017 5:20 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi Kim86, Sending entire string of character will result in tremendous delay. So such encrypted messages are used. The special character is not mandatory at all. U can use normal numbers also. The best way to assure healthy communication is using acknowledgement. I recommend the partner should respond with same data set which it has received eg. $100. Next data should be released after proper validating the previously sent data.Such scheme will not need any pause. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on