3/23/2011 9:40 PM | |
Posts: 6 Rating:
|
An upgrade to an ASI system has generated some questions about communications and errors detected using the ASI Interface Analyser.More details are included in the attached pdf. Typical ASI components: All components are new except Link 20E Master. 2 Safety Monitors, 6-8 D-I/O modules type 3RK1205 and 3RK1405, 10-13 E-Stops using ASI modules 3SF5500-0BA, 4-8 Pull cable devices model 3SF2 140-1BF00-0BA1. Topology: The ASI bus contains 25 slave devices and 2 Safety Monitors. Length 150 meters. The Power supply and Link 20E are located in a cabinet near the center of the network. Two main branches of ASI cable leave the cabinet, one to the left, the other to the right. On the longer ASI cable an Extension Plug is installed. Communication:
Reconfiguring ASI Node Addresses:
Questions: Link 20E Master:
AttachmentASI Communication problems.pdf (200 Downloads) |
Last edited by: O_Moderator at: 3/24/2011 10:21 AMnew subject after splitting |
|
2/6/2014 2:53 AM | |
Posts: 2 Rating:
|
nobody anwered this question? Regards darkdragos
|
Follow us on