4/29/2014 8:46 AM | |
Joined: 12/3/2012 Last visit: 6/26/2021 Posts: 4 Rating:
|
Dear All, I haved a problem when compile the CFC Chart with "Generate module driver" option is selected, but the corresponding parameters not connected and not assigned to mode channel of module ( EX: Mode, MS, CONN_TO_DRV,.....) - Figure 1: Hardware Configuration (used coverter DP/AS-i LINK Advanced : 6GK1 415-2BA20) - Figure 2: Compile the CFC Chart with "Generate module driver" option is selected, but the corresponding parameters not connected and not assigned to mode channel of module. - Figure 3: Document Interconnection diagram ASI. Thanks All, AttachmentInterconnection Diagram ASI.zip (42 Downloads) |
Follow us on