7/11/2007 8:12 AM | |
Posts: 112 Rating: (10) |
The FB125 diagnostic block also offers information of subordinate ASI bus systems, when a DP/ASI-Link is used as a DP slave, as mentioned in the online for FB125. See https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=CSEUS&objid=16740529for Siemens Protool/WinCC flexible screens that display the ASI information. |
7/14/2007 1:01 PM | |
Posts: 5822 Rating: (411)
|
Dear ashkya, you can never test HW Devices by a simulation Software. You always need Devices and PLCs to test. Best regards J_Bell |
7/19/2007 5:18 AM | |
Posts: 73 Rating: (20) |
Hello Ashkya, Using the FC_ASI_3422 block you can access the slaves command line interface. See the Link20E manual http://support.automation.siemens.com/WW/view/en/19549955 http://support.automation.siemens.com/WW/view/en/5281638See section 3.3 of the manual. I would assume that Report System Error FB49 would also be able to display diagnostic data for the ASI Slaves. FB49 uses Alarm S messaging |
Follow us on