3/31/2017 7:00 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Hello; I have not worked on As-i projects with the S7-1500 platform yet, but I have used the DP/As-i link 20E in a few occasions a few years ago (the module has been replaced since by the DP/As-i link Advanced, i believe). Basically, it is a Profibus-DP slave on the DP side, and, as such you need to integrate its gds file in your Profibus configuration software as a DP slave; you can then configure the As-i slaves that will be connected to it. The original CD that accompanied the module contained some sample programs, but I believe that at that time I believe they were for Step 7 v5.x, so they would not really help you for a S7-1500. The following linls will provide some guidance, you will find the DP/As-i link 20E manual, and a FAQ that provides a link to the gsd file you require (if it is not already part of the Profibus catalog of the Step 7 v13) and discusses how to setup the IO addresses of the As-i master. Configuring I/O addresses with DP-Asi link 20E Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/31/2017 7:13:57 PMLast edited by: dchartier at: 3/31/2017 7:31:31 PM |
|
This contribution was helpful to
1 thankful Users |
3/31/2017 10:09 PM | |
Posts: 3 Rating:
|
Thanks for your help I´ll read the arquives that you sugest to find the way |
Follow us on