6/18/2012 1:09 AM | |
Posts: 108 Rating:
|
Hi Darius, Unfortunately, it doesn't work for me. When trying to change the IP address of the PLC from 192.168.1.20 to 192.168.1.21, as described in my initial post, the PG IP address is 192.168.1.208. I have not been able to find any information on the error message that appears when I try to make the change: "The set command could not be executed." The attached zip file contains screenshots showing the screen at the following stages of the process of changing the IP address: 1 - Before changing anything. The IP address is 192.168.1.20 2- After entering the new IP address: 192.168.1.21 3 - After clicking "Assign new IP address". Error message: "The set command could not be executed." 4 - After going to a different page and returning. The IP address has returned to 192.168.1.20 and the IP address of 192.168.1.21 has been set as the router address, even though this option was never selected. Any ideas as to why this is happening and/or what can be done to resolve it? Jason AttachmentScreenshots.zip (1029 Downloads) |
Follow us on