9/14/2023 8:52 AM | |
Joined: 8/3/2009 Last visit: 2/11/2025 Posts: 14717 Rating:
|
Hello ProgrammatoriBiraghi in Unified you cannot assign Tags to properties you can always onld write a value of a Tag to a property. Every time you want to write a tag value to a property of a object you have to run the script. you can work with something like this to run through all objects of a screen to dynamise property values (LINK). but every time the value changes you would have to run the script again, And if you change the value ini any io field for example you would have to work with scripts here also to write the value back to the right tag.... So I think you should think about another general solution for your usecase. Perhaps a faceplate in Popup could be an option, here you can set tags to the interface and this works well in Runtime. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on