2/24/2013 1:41 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Use PST (Primary Setup Tool) New Primary Setup Tool (PST) version 4.1 and new version V3.2 or 4.0 for address setting of SIMATIC NET Industrial Ethernet products available for download Best regards, Hristo Mihalev |
2/24/2013 1:49 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Be aware that not all models do have an IP address. (X000, X100, XB000, ... don't). Only the manageable versions have an address (X200 and above). The MAC address that should react to device detection is the one printed on the device. Is the MAC used by the so called "Agent" in the device. When you use "edit ethernet node", do you detect all other devices except the Scalance Or no devices at all? Could be an indication where to search further. If you are unsuccessful with "edit Ethernet node", you could try the tool that is delivered with Scalance X itself, the primary setup tool. http://support.automation.siemens.com/WW/view/en/19440762 Node detection uses a protocol DCP, that you can disable by configuration in the switch or even in Step7. Extra note: When you say that a device has only one MAC, this is not true. For toplogy detection, each port uses a port specific MAC address (used by LLDP). But you will hardly detect thisaddress because it is only used between neighbour ports. And is not needed to set the IP address of the agent. |
Best regards |
|
This contribution was helpful to
1 thankful Users |
2/6/2014 10:48 AM | |
Posts: 1368 Rating:
|
Hello Vikram, if you do not want to use STEP 7, PST or WBM, you also can use the command line interface with the Windows Console. Look here http://support.automation.siemens.com/WW/view/de/63203259 Chapter 4.2 Greetings, |
2/6/2014 11:18 AM | |
Joined: 10/17/2011 Last visit: 1/28/2025 Posts: 3 Rating:
|
Thank you for the information,it was really useful. |
7/30/2014 4:13 PM | |
Joined: 9/1/2005 Last visit: 3/10/2025 Posts: 4113 Rating:
|
follow up question published by Tomas123is split to a seperate thread with the subject SCALANCE W788 - cant log in by the browser. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
6/12/2015 2:39 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by AAB_11429 is split to a separate thread with the subject Scalance X206-1, configured the IP Address.
|
Follow us on