6/10/2020 9:58 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077)
|
Some this like this simple example?
AttachmentPercent_to_output_0BA8.Standard.zip (265 Downloads) |
This contribution was helpful to1 thankful Users |
6/11/2020 10:30 AM | |
Joined: 11/11/2017 Last visit: 5/3/2024 Posts: 187 Rating: (4) |
its a start and thanks but i really need to have the pulse timed both off and on for the heater to maintain the heat |
6/11/2020 10:36 AM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077)
|
You give only minimal Information. You know what you want, I not. |
6/11/2020 1:46 PM | |
Joined: 2/22/2008 Last visit: 5/8/2024 Posts: 2698 Rating: (206) |
The point is, that the PWM is the ready to use function for your application, but you have not tested the example. Your table shows a linear characteristic and the PWM will automatically use the right on and off times, if you use proper parameter. PWM1 Try out with different percent values. Switch on I1 and wait, until the on time is over. Then you can see measured time in the display. The right part of Q1 is only needed for simulation and displaying the on-time of Q1. PWM2 This is with an impulse generator, but calculated values instead of a table. Regards, Scorp AttachmentPWM.zip (260 Downloads) |
This contribution was helpful to1 thankful Users |
6/11/2020 2:54 PM | |
Joined: 3/30/2020 Last visit: 5/9/2024 Posts: 4491 Rating: (941) |
Hello. The application sounds like something where one would use a PI temperature controllers for. Siemens has some example on temperature control that would apply. Side note.. The "Application example" link does not work on the above page. The actual page is now [LINK]. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
6/11/2020 3:11 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077)
|
I say: Either you haven't dealt with block "PWM" yet or you don't understand how it works. |
6/11/2020 3:53 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077)
|
Attached is a example with entering the percent per LOGO! display. AttachmentPercent_to_output_0BA8.Standard_V2.zip (220 Downloads) |
This contribution was helpful to1 thankful Users |
6/11/2020 4:33 PM | |
Joined: 11/11/2017 Last visit: 5/3/2024 Posts: 187 Rating: (4) |
quick question: is there anyway to display the both off and on time on the TDE? |
6/11/2020 4:35 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077)
|
See post above your last post.... |
Follow us on