Industry Online Support
Technical Forum
1/4/2010 9:14 AM | |
Posts: 5 Rating:
|
Dear all I have a project that use S7-300 CPU as field controller and SIMATIC NET OPC as OPC server, all I need is to test the whole project offline before buying anything.I need just to insert the symbol table of the S7-300 station to the OPC offline i.e. (without real CPU), I tried many ways some of them were included in the following link (https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=17413251&caller=view ) but always there is error, so is it possible to read this symbols with the OPC with no CPU installed. |
1/4/2010 11:49 AM | |
Posts: 5 Rating:
|
Dear neo i did all what you told me but no symbol was loaded to the symbol configrator |
Follow us on