7/3/2023 9:38 AM | |
Joined: 2/3/2022 Last visit: 9/27/2023 Posts: 249 Rating:
|
Hi! Could you share with us the version that you are using? Br! |
7/4/2023 6:12 AM | |
Joined: 11/4/2021 Last visit: 9/28/2023 Posts: 7 Rating:
|
I tried with V17 update 6 and V18 update 1 In the MTP700 I tried Operating system 16 and 18 Now the situation is like in the photos Thanks AttachmentUnified.pdf (44 Downloads) |
7/10/2023 5:32 AM | |
Joined: 11/4/2021 Last visit: 9/28/2023 Posts: 7 Rating:
|
Any update ? Thanks |
7/11/2023 5:23 AM | |
Joined: 1/21/2013 Last visit: 9/29/2023 Posts: 2084 Rating:
|
Hi daniele.gemignani, It would help us to know exactly what you are struggling with. You are referring to video timestamp 0:45. This is where the VLC media player shows the available audio devices. Your screenshot only shows the default devices. This would indicate that you have not connected a supported audio device. The "cards" file shown at 4:32 will always contain "PCH" and "pcsp". If there is a 3rd entry, use it. You should be aware that the device names depend on the hardware you are using. I tested with a Sennheiser PC 8 USB and for that headset the card is named "headset". Kind regards |
Follow us on