5/19/2022 3:16 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello Sharky50 you can use PM Open Export for this Usecase. Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/20/2022 12:41 PM | |
Joined: 5/1/2020 Last visit: 4/24/2025 Posts: 72 Rating:
|
Hello, edit i run your code the issue is with the active screen one solution that worked out for me assuming you still want to keep the alarm screen as a screen and not a screen window all but invisible everywhere is the following two scripts.What i did was change momentarily the basescreen to another screen where i had the alarmcontrol (that's NewPdl0) and i saved the screen name to an internal tag(testing) plus set a bit (testbit) that is the event trigger for the second script which just changes my active screen from the alarm screen to what it was plus resets the bit I did this on wincc v7.5 so i think you have to change hmiruntime.tags to hmiruntime.smarttags maybe i ll check later on my wincc proffessional vm Attachmentexportalarmscsv.txt (496 Downloads) |
Last edited by: Gdim93 at: 05/20/2022 14:30:05 |
|
This contribution was helpful to
1 thankful Users |
5/20/2022 2:38 PM | |
Joined: 10/29/2020 Last visit: 4/25/2025 Posts: 7 Rating:
|
Good morning, I got this error: Get_Item: get parameter is incorrect. Thank you very much for your help. |
5/20/2022 3:35 PM | |
Joined: 10/29/2020 Last visit: 4/25/2025 Posts: 7 Rating:
|
Thank you so much for your help. It's working great. |
Follow us on