10/27/2020 10:23 AM | |
Posts: 1 Rating: (0) |
Hello, i need some help. Accordingly to SIEMENS TOPIC, it is possible to log in directly with a user-defined website. I use a 1215C DC/DC/DC CPU with firmware V4.2 and TIA Portal Professional V14 SP1. In the user administration the user Everybody has all rights. Nevertheless I get the message user Everybody must have access right 'open user-defined web page'! I have checked this several times and the hook is set. Unfortunately I do not know where the error is. Is this a known error or is something wrong configured ? Nevermind, i found the issue. Apparently the access level has to be on full access to allow all users the access. |
Last edited by: UphausKrone at: 10/27/2020 11:04:39Last edited by: Jen_Moderator at: 10/27/2020 12:48:23Optimized link. |
|
This contribution was helpful to2 thankful Users |
1/7/2021 1:35 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello UphausKrone, there is an FAQ in the internet and it could be useful for you: How can you directly access user-defined web pages of the S7-1200 / S7-1500? With best regards |
Follow us on