4/21/2009 7:49 AM | |
Posts: 487 Rating:
|
Hi Got a problem connecting via remote desktop to a wincc PC . Actualy the problem is after I disconnect.When you disconnect , the window loggon screen appears and the operator has to loggon again which is no good because due to user rights ( required for wincc) the operator does not know the password for that user.When the PC starts up there is an autologgon . Is there a way to do a autologgon after disconnecting via remote desktop. This problem is related to the following link Greetings Eric |
Last edited by: aikona at: 4/21/2009 8:11 AMLast edited by: aikona at: 4/21/2009 8:10 AM |
|
4/21/2009 10:51 PM | |
Posts: 2661 Rating:
|
Hi Eric, You can implement auto logon in Windows by making modifications in the Registry. See following FAQ: How can you implement an automatic logon (Autologon) in Microsoft Windows? |
4/22/2009 9:41 AM | |
Posts: 487 Rating:
|
Hi Yes the PC has an autologon,but instead of using the siemens way i used a microsoft program called Tweakui No a reboot is out of the question...but we did find a solution Made a little batch file I put on the desktop content of RMT_Disconnect.bat : 'tscon.exe 0 /dest:console ' This disconnects the remote user and restores the user on the PC Greetings Eric |
This contribution was helpful to
1 thankful Users |
Follow us on