6/23/2009 11:04 AM | |
Joined: 5/28/2008 Last visit: 3/20/2023 Posts: 4384 Rating:
|
Dear WinCC, Please note that PC/MPI-Adapter and USB/MPI- Adapter are not relesed for transfer of this panel. Here's attached a docment descriping all relesed cables for transfering projects to Siemens Panels. Also have a look on the following FAQ: How do you backup/restore with a Windows-based panel? Regards, AttachmentProjekttransfer_e_C1.pdf (134 Downloads) |
Ayman Elotaify |
|
6/23/2009 11:10 AM | |
Joined: 3/21/2006 Last visit: 3/2/2023 Posts: 10221 Rating:
|
Hello, To prepare bakup of this panel you could use Prosave (you can' edit backup, only restore on the same type of panel) or WinCC Flex (you can edit backup file) but if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". About necessaries cables look at What transfer options are available in the various operator panels? How to use Prosave to prepare backup look at How do you backup/restore with a Windows-based panel? Hope this will helps. Best regards Hristo Mihalev |
7/2/2009 7:18 AM | |
Joined: 6/3/2009 Last visit: 2/20/2023 Posts: 99 Rating:
|
Dear all I got it what i requried. |
Follow us on