4/6/2018 9:31 AM | |
Joined: 10/15/2016 Last visit: 3/21/2025 Posts: 90 Rating:
|
Hi all, I need some help with a Bar Code scanner on a S7-300, CP340 Card with RS232 ASCII protocol. I have 1 Scanner and need to read 2 bar codes which will then be compared and stored until reset. My programming skill is very basic at the moment and can only understand ladder for now......i know strike me down. I have used P_RCV and have managed to get 1 bar code where i want it (I think). i just cant for the life of me workout how to correctly scan a 2nd code into a different data area. I have attached a library with my code, just need someone to have a look and point me in the right direction. Code has some missing parts as i don't have conditions yet. Thank You AttachmentSCANNER_CODE.zip (220 Downloads) |
Follow us on