9/17/2017 1:29 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
Most of all I'm worried about the motor BAUMULLERDSO 100-L SYNCHRONOUS MOTOR, FORCED VENTILATION, RESOLVER 2000rpm, 19.2kW, 32A, 84Nm on nameplate is written Uzk=540V It's like servo motors 1FT7… but the family 1FT7 does not have a motor similar in characteristics 2000rpm, 19.2kW, 32A, 84Nm so I chose 1PH8 (SYNCHRONOUS MOTOR)… and I'm worried that the dynamic characteristics 1PH8 slightly worse than 1FT7 (for example, the task of making one revolution of the motor (360) - stop -and immediately reverse back at maximum speed) |
9/18/2017 3:42 PM | |
Joined: 10/11/2006 Last visit: 9/30/2024 Posts: 5909 Rating: (805)
|
Hello, you can use "Sizer" to size motor and drive. https://support.industry.siemens.com/cs/ww/en/view/54992004 |
With best regards, |
|
Follow us on