5/2/2017 8:26 AM | |
Posts: 3 Rating:
|
Hi i need help about networking on S7 1200 ,have 2 CPU 1214C every with their HMI panel KP 300 MONO. We can say that they are independent system. Only what i need more is sending one Byte from CPU 1 on CPU 2 .. Which communication is best to use and if HMI connection and local/partner connection must be on same subnets or not thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/2/2017 5:02:02 PMNew subject after splitting |
|
5/2/2017 10:08 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi zjurdik, You can comunicate over S7 connection with the blocks PUT/GET. This FAQs may help you: How you configure a connection in the TIA Portal? You can also communicate over I-Device. See this application sample: Configuration and application of PROFINET I-Device function hope this helps, regards, |
Last edited by: mopS04 at: 5/2/2017 10:08:57 AMFCK WAR! |
|
5/14/2017 8:00 AM | |
Posts: 24 Rating:
|
hello, the below document, is getting start one and is so helpful for you, plz read it. please push the rate button, if it is helpful for you. https://support.industry.siemens.com/cs/attachments/73505596/GettingStarted_en-US.pdf?download=true |
Last edited by: Min_Moderator at: 5/15/2017 3:50:41 PMReplace link |
|
Follow us on