2/5/2018 2:14 PM | |
Joined: 8/15/2011 Last visit: 9/9/2024 Posts: 145 Rating:
|
Hello, a very interesting idea... any solutions found? SIMATIC NET OPC Server is the Best.? (for Siemens PLCs...) |
2/17/2018 11:51 AM | |
Joined: 9/9/2011 Last visit: 2/25/2025 Posts: 102 Rating:
|
Hello I have the same problem too : I have principaly 3 types of products : - Products in MODBUS TCP : i use OPUA PROSYS : (good price and no need to pay maintenance cost every year). Free test can be done for 1h, need to restart server. https://www.prosysopc.com/products/opc-ua-modbus-server/ - SIEMENS S7-1200 : SIMATIC NET.(V12 and V13) principaly. working well more exactly when there is some siemens updates .... I prefer to keep Simens in this case and tell theim problem in case of. It's easier than to other external server For each program need only to make a S7 Link and don't forget to include PUT-GET. You can put all variables access in each program. (or make an individually choise) Or in the SIMATIC NET edit variables for each PLC and delete variables not need... - Kep Server for OMRON PLC. (quite expensive). A lot of other drivers possible, each driver can be payed individually. |
Last edited by: GB002 at: 2/17/2018 11:53:05 AMLast edited by: GB002 at: 2/17/2018 11:54:19 AMLast edited by: GB002 at: 2/17/2018 11:54:38 AMLast edited by: GB002 at: 2/17/2018 11:55:15 AMLast edited by: GB002 at: 2/17/2018 11:55:36 AMLast edited by: GB002 at: 2/17/2018 11:56:17 AM |
|
5/8/2018 3:56 PM | |
Joined: 8/3/2009 Last visit: 3/26/2025 Posts: 15084 Rating:
|
Hello If your Systems also have a WinCC HMI running then you can use the OPC Server functionality of the HMI Runtimes (Comfort Panel, WinCC Professional RT or WinCC Advanced RT, it takes no additional license). But in that case you need a OPC Client Application that gather the needed Signals and Data from all the HMI OPC UA Server and write it into SQL Server. (First Result from goolge Industrial Data Bridge is also an option we used before. its quite easy to set up. you do not have to program anything you can click your project together (you also can use it standallone without WinCC!!!). Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
5/9/2018 9:34 AM | |
Joined: 5/31/2011 Last visit: 2/11/2025 Posts: 190 Rating:
|
About the link you provided: Looking at the specs it seems it is for OPC-DA. We only will be using OPC-UA. KepserverEX is also a stabel solution I've been testing. But I'm now installing IndustrialDataBridge on our test system. I'll post back my findings (if I don't forget)... |
Last edited by: ThaKibosh at: 5/9/2018 9:34:58 AM |
|
5/9/2018 9:40 AM | |
Joined: 8/15/2011 Last visit: 9/9/2024 Posts: 145 Rating:
|
hello, here some info from Industry Online Support: Application example https://support.industry.siemens.com/cs/de/en/view/109483465
|
Follow us on