6/25/2016 9:12 AM | |
Posts: 4 Rating: (0) |
hy there, I'm having a problem on the SF in solid red but the BF flashing red. What should i do? this happened when the rs232 was accidentally plugged into the DP port. i try to connect and go online but seem that i can do it. do i need a special cable to do the communication ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/27/2016 3:04:17 PMNew subject after splitting |
|
6/25/2016 9:24 AM | |
Posts: 4 Rating: (0) |
hy, thanks for the reply. i have a RS232 adapter and yes im using 315-2dp and an slave connected between the 315 and hmi |
6/25/2016 9:34 AM | |
Posts: 4 Rating: (0) |
yes i connected it to the left port but everytime i tried to go online it said no connection. do i need to do some setting? |
6/25/2016 9:37 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, OK You have this Adapter 6ES7 972-0CA23-0XA0? Is there a check list for implementing a PC adapter? - ID: 10420976 ... |
6/25/2016 9:44 AM | |
Posts: 4 Rating: (0) |
oh no.... dont have that, will look for it and try to go online. thanks |
Follow us on