8/2/2010 9:05 AM | |
Joined: 7/28/2010 Last visit: 4/25/2023 Posts: 184 Rating:
|
Sinec911, The only data which should be on the EPROM is Siemens Code which is in the S5D code. Could you tell me why you want to transfer Hex code to EPROM? Regards, Behnam www.sigmaprocess.ca |
8/10/2010 9:18 AM | |
Joined: 7/28/2010 Last visit: 4/25/2023 Posts: 184 Rating:
|
Sinec911, I doubt you can downloadthat .hex file. EPROM for CP521 can be programmed through COM 521 which can be used with Step5 V6.x The type of file you can load through COM521 is called Basic (*.bas). Take a look atchapter 5 in the attached file for manual on COM521 software. Regards, Behnam www.sigmaprocess.ca Attachment6ES5 998-0UW21.pdf (131 Downloads) |
8/10/2010 10:36 AM | |
Posts: 6 Rating:
|
Dear Behnam, Thats right, its impossible to use the Step 5, i need to get someone, who has the COM 521 basic to complete this. thank you |
8/25/2015 1:03 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4814 Rating:
|
New question published by Harish G is split to a separate thread with the subject Converting old S5 system to S7, CP timeout. Best regards |
Follow us on