9/23/2015 3:15 PM | |
Posts: 739 Rating:
|
To save Parametersets into the BOP belongs to the BOP you have.
6SL3255-0AA00-4CA1 G120 BASIC OPERATOR PANEL (BOP-2) The extras menu allows the user to perform the following functions: ● DRVRESET - reset the Inverter to the factory default settings. ● RAM ─> ROM - copies data from the Inverters RAM to the Inverters ROM. ● FROM CRD - reads parameter data from the memory card into the Inverter memory. ● TO CARD - writes parameter data from the Inverter memory on to the memory card. ● FROM BOP - reads parameter data from the BOP-2 to the Inverter memory. ● TO BOP - writes parameter data from the Inverter memory to the BOP-2. https://support.industry.siemens.com/cs/ww/en/view/42185248
6SL3255-0AA00-4BA1 G110/G120 BASIC OPERATOR PANEL (BOP) Parameter sets cannot be saved
6SE6400-0BE00-0AA0 MM4 BOP-2 BASIC OPERATOR PANEL 2 Parameter sets cannot be saved |
This contribution was helpful to
3 thankful Users |
9/24/2015 2:04 PM | |
Posts: 4 Rating:
|
Thank you very much for the in-depth reply! |
Follow us on